Print Documents in Bid Manager

There are three methods for printing documents in Bid Manager:   Documentation Service, Quick Print, and PDAS. 

·         The Documentation Service is designed to assist with compiling job related documents from one or more job alternates together into a complete PDF document package.  External documents can be added into this package, and many standard documents are available for selection.  The compiled PDF document can be downloaded from the documentation service server using a link provided via email. 

·         The Quick Print function allows the user to print a bill of material, bid manager drawings, and price sheet (some users may also include MI information).  

·         The PDAS option emails the AutoCad submittal drawings and XML information that can be used in Design Automation.


Procedures in this Job Aid:

·         Open the Documentation Service

o    Enter the Job Information

o    Select Documents

o     Common Library and Document Library

o    Common Library

o    Document Library

o    Configure the Package

o    Submit the Package

·         Quick Print

·         PDAS

·         Set Defaults for Displaying Pricing and Header/Footer Information

·         Document Print Queue

 


Step 1: Open the Documentation Service

There are two ways to open the documentation service; from the home screen of Bid Manager, or within a job.  If you access it from the home screen, you must specify a job you want to print.

1.     Click on Create Document Package from Actions area in the home screen.

2.     Or, find and open a job. 

3.     Click on an existing alternate from the Overview left side tab.

4.     Click on the Document Service button in the Home top tab.


Step 2: Enter the Job Information

1.     When the Document Service is accessed through the job screen, the alternate that was selected will be populated in the Document Service.  To add an additional Bill of Material (Alternate) to the documentation service, type a General Order (GO) Number, Negotiation (Neg) Number, Job Name, or Sales ID in the Add job search field and press the search button.           

 

Note: To remove alternates, click on the trashcan icon next to the alternate name.

2.     In the search results, place a check mark next to the alternates to include them in the document package.

Note: The Data Location column displays the location where the job is stored. Jobs are listed in rows, and Orders are shown in Green rows. If a job shows up in multiple data locations, all copies of that job are shown.

3.     Change the Job Reporting (Quote Type and Status) and Regional Settings (Language and Currency Format) in this tab as well.


Step 3: Select Documents

In Tab 2 of the documentation service, the document package can be customized to include specific documents.

1.     Select the Organize Items By menu to choose the order in which the items should appear.

·         Power Flow selection will order the products from highest voltage to lowest voltage by product type (Switchboard, Panelboard, Safety Switch…)

·         Item Number selection will order the products by their item number that was assigned in the Edit Items screen.

2.     Optionally, select a Standard Document Package. Standard Document Packages apply a template of documents to the document package that can be further customized using the choices below it.

Note: If you select Full Bid or Quick Bid, you will be required to complete the information in the Enter Additional Information tab on the right side because a proposal letter will be included that requires an Addressee.

3.     Customize the package by using the drop down menus next to each document type and changing the selection.

 

Main Documents

Action

Proposal Letter

Select the type of proposal letter.

Title Page

Select a title page format.

Table of Contents

Select with or without page numbers.

Combined Bill of Material for All Items

Select None or a level of detail for the combined Bill of Material that will be included in the front of the document as opposed to the more popular Product Line Bill of Material.

Selling Policy

Select None or a Selling Policy.

Comments and Clarifications

Select None or Standard

Product Line Specific

Action

Separate Bill of Material by Product

Select a level of detail for the Bill of Material - Detailed (used most frequently), Intermediate, Summary or None.

Drawings

Select a type of drawing format. Note: this drives what is printed on the Bidman drawings.

Literature

Select a type of literature:

Submittal: Technical Data folder

Submittal & Instructions: Adds the product line instruction IL in a folder.

O&M: Instruction, Component, Renewal parts folders.

O&M & Technical Data: Adds Technical Data folder to the above

Document Package Specific

Action

Product Line Pages

Select to be included. This includes a page with the Product Line name, such as Panelboards.

Product Line Table of Contents

Select standard with or without page numbers.

Sub tab Pages

This provides a Tab page with the folder names (as selected under Literature)

Small Projects Template: For submittals, only included the Technical Data sub tab.

Literature Divider Pages

Puts an Eaton Logo blank page between different literature items.

Maximum Binder Size

Select a binder size for printing. Binder size will limit the number of pages in the pdf and create multiple volumes per the selection.  (3 inch is the default)

Note: To show a price in the document package, a Bill of Material must be selected in the Main Documents and the Document Formats must be selected to show price in the My Account tool.

Note: The Table of Contents tab on the right side shows the documents that will be included in the package and the order that they will appear.

Common Library and Document Library –EatonCARE and CTC ONLY

EatonCARE and CTC employees will have access to the Common Library and Document Library. These libraries contain documents and literature that can be added to the document package. 

Common Library

Commonly used documents organized by Product Line. 

1.     Select/Highlight the folder that the document will be included in.

2.     Select the product line drop down menu in the common library.

·         Optionally, select a filtering option.

3.     Select the document to be added.

4.     Click the + Add Document button.

Document Library

This is a General search in Enovia, only available to internal EatonCARE and CTC Users.  It allows a search of all in Enovia documents.

1.     Select/Highlight the folder that the document will be included in.

2.     Select for the file in the document library.

3.     Select the document to be added.

4.     Click the Add to Document Package button.

Step 4: Configure the Package

In Tab 3, rearrange, customize or delete documents selected in Tab 2.  Folders can be added to group documents.  External documents can also be added in this tab.

1.     The left section of the window displays the folder structure of the package. 

2.     Select a document, and use the buttons in the ribbon bar to configure the document package.

Note: The red warning icon next to the Main Documents folder indicates that there is additional information to complete before submitting the document package.

Button Group           

Button Name

Description

Package

Save

 

Reset

Save the package in order to return to at a later time.  Packages can be saved for each type. Note: Only one save per type.

Resets any saved package and returns to default choices.

Edit

Cut

Paste

Rename Folder

Rename Job

Cut a folder or document

Paste the cut folder or document

Rename the selected folder. (E.g. Panelboard Spec Section 16492)

Provides 3 lines of text (50 characters each) to replace the Job name in all references.

Actions

Add Folder

 

Add File

Replace

Preview

 

Apply Placeholder

Add a Product Line Folder to be customized by user.

Add a file from a local drive

Replace selected item with another

Preview document (Documents can be previewed in XPS)

When a plant drawing is missing, a placeholder is available. This is a global placeholder selection.  This can be changed on an item level basis as well.

Display

Expand

Collapse

Expand the folder view

Collapse the folder view

Re-Arrange

Move up/down

Move top/bottom

Move by one line at a time

Move to the extreme top or bottom of order

3.     Documents can easily be moved from folder to folder by dragging and dropping in the list.


4.     Select or unselect items with the check mark box next to the item to include or remove the document in the final package. 

5.     External files can be added into the document package by using the + Add Document button. Files will be added into the folder that is currently selected. The file name of the document added will appear on the Bill of Material.

6.     Select a document and click the Preview button to see a preview of that document.

Note: Documents loaded in formatter on classic Bid Manager jobs will show in the Technical Documents folder. If the plant has loaded drawings, the item folder will end with the number of drawings and the title of the plant release type: Approval, Confirmation, Construction, or Final.


7.     If plant drawings have been requested for an Item during order entry, but no drawings are available, a warning triangle  will appear in front of the item.  This triangle indicates some form of placeholder is required. A placeholder type must be defined to submit the package.  A Placeholder inserts a page with the item number and designation.

·         Placeholder – Inserts a placeholder page.

·         Bidprint drawings - inserts the bidprint drawings from Bidmanager.

·         Bidprint BOM - inserts the bidprint Bill of Material from Bidmanager.

·         Bidprint BOM + Drawings - inserts both the bidprint Bill of Material and drawings from Bidmanager.

The placeholder page has a red border to indicate something is missing:

 


Step 5: Submit the Package

In tab 4 of the documentation service, additional information may be required before submitting the package that information will be highlighted in red. The document package will be created in a PDF format that will be available for download via a link provided in an email response. If the package is less than 5MB it can be requested as a pdf attachment in the email with the link. The document package will be available for 72 hours using the provided link. After 72 hours, you will need to resubmit the package as links cannot be refreshed.

1.     Enter the email address to which the document package link will be sent to.  Additional email recipients can be added here, or the email with the link can be forwarded after it has been received and reviewed.

2.     Optionally, place a checkmark to not include missing file placeholders.

Note: Missing file placeholders are included when a file or drawing cannot be retrieved from Enovia. These are different placeholders than on Tab 3 for drawings not yet available.

3.     Use the radio buttons to choose to receive the final document as a link only or as a pdf and a link. 

Note: Files over 5MB will only be sent as a link.


4.     In the Enter Additional Information tab under the Customer Information, Bid Manager imports the customer information that was selected when the job was created.  To populate the customer information fields with a customer that was originally added to the job, click on that customer name from the Current Selections tab. To add new customer information to the document package, click on the Search tab.

5.     Fill out all required fields that are titled in red.

6.     Click the Submit button.

Note: If the submit button is grey and unavailable; information may be missing from the previous tabs.  If information has been entered in the past, Bid Manager will attempt to auto populate the fields when text is being entered.

Email Response and PDF Document

The email response from the submitted document request will include a link where the document is available for download for 72 hours.  This link can be forwarded to any desired recipient.


Links to the files (volumes) that have been formatted for printing will show according to how the document binder size was selected.

·         The electronic copy shown above for a submittal combines all volumes into one file.

·         The electronic copy for an O&M removes the blank pages and combines all volumes into one file.

·         The rest of the links are for use in printing a document.

Quick Print

Quick Print allows you to quickly send or receive a bill of material and approval drawings. Bid Manager will email a bill of material in Word format, and the approval drawings in PDF.

1.     Open an existing job or order copy in Bid Manager and select an alternate.

2.     On the Home top tab, click the Quick Print button.

3.     Enter the email address of the recipient. Select BOM, Approval Drawings or BOM + Approval Drawings.  Some users will also have the option to Include Price Sheet, or MI.

4.     Click the Quick Print button to email the selected items to the recipient.

Note: Depending on your account type you may not see all the options listed here. When the MI box is checked the Manufacturing Information is included in the Approval Drawings PDF.

5.     Check your email program for an email from ManualNotification@eaton.com, Bid Manager Documentation Service (Quick Print).  Open the email and save the attachments to your computer. 

6.     Optionally, open the Bill of Material in Word, and edit as necessary.


7.     Optionally, edit the Approval Drawings PDF with any PDF editing software. The Manufacturing Information will be included in the Approval Drawing PDF.

 


Open a Pricesheet in Excel

When Quick Print emails a copy of the price sheet the file sent is in an XML format. This file can be opened using Excel, however if you have never used Excel to open an XML file you will need to follow the steps below to set Excel as your default XML program.

1.     Open the email sent by ManualNotification@eaton.com, Bid Manager Documentation Service (Quick Print), and then save the PRICESHEET.xml file to your computer.

2.     Right-click the PRICESHEET.xml icon on your desktop and select
Open with ® Choose default program.


3.     When the Open with windows opens select Microsoft Excel, and then check the Always use the selected program to open this kind of file box.

4.     Click OK, and Excel will open the XML file.

5.     Click Enable Editing to edit the price sheet information, and click the Save button the file to save any changes.

6.     All future Pricesheets will now open in Excel automatically.

 


PDAS

PDAS allows users who need to edit submittal drawings to receive a copy of the AutoCad file via email.

1.     Navigate to the Items tab in an open job.

2.     In the Items tab, select the necessary products.

3.     Under Documentation, click the PDAS button.

4.     Enter the recipients email address, and click the icon below the email field.

 


5.     An email from ManualNotification@eaton.com containing the XML file, and a ZIP file containing the Autocad drawings will be sent to your inbox.

Note: A file archive program such as WinZip or 7Zip will be required to open the zip file attachment.

Set Defaults for Displaying Pricing and Header/Footer Information

You can control which price prints on a Bill of Material, and at what level the price is displayed.

1.     In the Home screen, click the My Account button.

2.     Click on the Document Formats tab.

3.     The Document Formats tab allows you to choose the pricing information and which level of the bill of material will appear on a bill of material from Quick Print and Document Services. Select from the options listed in the table below:

Document

Drop Down Options

Quick Print Pricing

No Pricing Information – Creates a BOM without a printed price.

Quote Price – Displays the price for the end customer
(Market List Price x Your Multiplier x Quote Multiplier = Quote Price)

Market List – Displays a takeoff price without any multipliers applied. 

Display Item Pricing Only – Displays line item pricing

Display Total Pricing Only – Display a subtotal for all items

Display Item and Total Pricing – Displays line item pricing along with subtotals

Quick Print BOM Level

Summary – Creates a BOM with the job information, item numbers, quantity, product family, product description, catalog numbers, and designations.

Intermediate - This option will only be different for certain products. Otherwise this is option is the same as Summary.

Detailed – Creates a BOM with all the information from the Summary & Intermediate BOMs plus a list of materials broken down by item.

Document Service Pricing

No Pricing Information – Creates a BOM without a printed price.

Quote Price – Displays the price for the end customer
(Market List Price x Your Multiplier x Quote Multiplier = Quote Price)

Market List – Displays a takeoff price without any multipliers applied. 

Display Item Pricing Only – Displays line item pricing

Display Total Pricing Only – Display a subtotal for all items

Display Item and Total Pricing – Displays line item pricing along with subtotals

4.     Click Configure to change the default settings for the document output including footer options.

5.     Click OK.

6.     Click Save.

7.     Close the My Account screen.


Document Print Queue

After submitting a request for a Document Package, Quick Print, or PDAS file package the Document Print Queue shows where the request is in the Documentation Service Print Queue.

1.     Add the Print Queue tool to your Bid Manager homepage (See Navigate Bid Manager and Customize the Homepage job aid for more information).

2.     On the Bid Manager homepage, click the Document Print Queue button.

3.     When the Document Print Queue opens, you can find your requests by entering the

·         Requestor Sales ID (Bid Manager ID, which is also the first four characters of a Neg Number).

·         Locator (GO# Neg#)

·         Start Date (Date the document service was requested)

4.     Click the Search button.

5.     Search results can be grouped by Date, Requestor, or Locator.

6.     Search results can be exported to Microsoft Excel.